Technical FAQs

Ask a Question

Can a Lock Kit be added to the cover of the QO312L125G load center?

Issue;
Product design features

Product line:
QO load centers

Environment:
product accessories

Cause:
Application

Resolution:
Yes, use PK6FL. Two keys are provided with this lock kit and  a replacement key is also available, catalog number LP9618.


CTA-ID : 2000506
Was this helpful?
What can we do to improve the information ?