Technical FAQs

Ask a Question

What cable sizes can be used with lugs for the UL 489 listed M9 breakers?

Cable range: pressure terminals are suitable for copper cables:
0.5 to 25 A: #18 to #4 AWG
32 to 63 A: #18 to #2 AWG


CTA-ID : 2000203
Was this helpful?
What can we do to improve the information ?