Technical FAQs

Ask a Question

Is the UL 489 listed M9 breaker available with a combination of box lugs and ring tongue terminals?

Yes. You may get box lugs on the line side, and ring-tongue terminals on the load side. They are NOT available with box on the load side and ring on the line.


CTA-ID : 2000202
Was this helpful?
What can we do to improve the information ?