Technical FAQs

Ask a Question

Does the UL 489 listed M9 breaker have a 480 Vac Delta rating?

No. The 480 V UL 489 listed M9 breakers are rated for 480Y/277.


CTA-ID : 2000194
Was this helpful?
What can we do to improve the information ?