Technical FAQs

Ask a Question

What is the termination temperature rating of a QO breaker?

QO breakers rated 10 to 30 amps, GFI, AFI breakers are suitable for use with 60 deg C or 75 deg C wire. QO breakers rated 35 to 125 amps are rated for use with 75 deg C wire only.


CTA-ID : 2000192
Was this helpful?
What can we do to improve the information ?