Technical FAQs

Ask a Question

What is the replacement 600A 3P main breaker ``top mounted`` for HCM3674-6M?

Issue:
What is the replacement 600A 3P main breaker ``top mounted`` for HCM3674-6M?

Produce line:
I-Line panelboards and accessories sold and supported in the USA.

Environment:
Selection 

Cause:
Replacement

Resolution:
You can use an MAP36600 and reverse the lugs for top mounting, or you can use an MAL36600 and remove the lugs from the load end.

Note:  The MAP/MAL breakers are now obsolete with no replacement. The entire panelboard will now have to be replaced.


 
Was this helpful?
What can we do to improve the information ?