Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H92356 Double Throw Safety Switch?

The lugs on this device will accept (2) #4 AWG - 500 kcmil aluminum or copper conductors per phase. Although the lug will accept 600 kcmil conductors, the wire bending space available in the switch restricts the maximum to 500 kcmil conductors.


CTA-ID : 15575
Was this helpful?
What can we do to improve the information ?