Technical FAQs

Ask a Question

What is the part number for the secondary ring nut that holds the knob on a K or SK selector switch or potentiometer?

9001 SK46 is part number for the secondary ring nut.


CTA-ID : 15302
Was this helpful?
What can we do to improve the information ?