Technical FAQs

Ask a Question

What size of mounting screw is used with the PKxxGTA equipment ground bars?

Issue:
Repair Parts

Product Line:
LC Accessory

Cause:
Maintenance

Resolution:
The ground bar mounting screw(s) is an 8-32 x .688`` pan head (phillips drive) THREAD FORMING screw. Do not substitute a SELF TAPPING screw. To purchase the mounting screw, order part number 2159414220.


CTA-ID : 15030
Was this helpful?
What can we do to improve the information ?