Technical FAQs

Ask a Question

What is the Terminal Lug Data for a 92355 Double Throw Safety Switch?

The lugs on this device will accept (2) #4 AWG - 250 kcmil aluminum or copper conductors per phase. Although the lug will accept 350 kcmil conductors, the wire bending space available in the switch restricts the maximum to 250 kcmil conductors.

CTA-ID : 15556
Was this helpful?
What can we do to improve the information ?