Technical FAQs

Ask a Question

What is the catalog number for a ``HL`` limit switches - hi ambient temperature type of 350 degrees F?

Order L100 or L300 type, add ``H`` to the prefix for ``housing options - high temperature O to 350 degree F``, per Digest 172, pg. 19-23.

CTA-ID : 15291
Was this helpful?
What can we do to improve the information ?