Technical FAQs

Ask a Question

Can you get an NQOD panelboard, 225A maximum,with feed thru lugs in a 14 inch wide enclosure?

Feed thru lugs can be provided on a 14 inch wide, 225A, NQOD panelboard. The panel must be factory assembled and is limited to interiors that will fit into boxes up to and including a height of 56``.

CTA-ID : 15284
Was this helpful?
What can we do to improve the information ?