Technical FAQs

Ask a Question

What Tenant Circuit Breakers can be used with a MP43200, MPR43200 or MPH43200 Meter Center?


Product Line:
MP Meter-Pak

Application of tenant breaker

These Meter-Pak Meter Centers accept QOM2-MM (10,000 AIR) or QOM2-MVH (22,000 AIR), 100 ampere through 200 ampere, tenant circuit breakers.
Example Catalog Numbers are:
100A = QOM2100MM or QOM2100MVH
125A = QOM2125MM or QOM2125MVH
150A = QOM2150MM or QOM2150MVH
175A = QOM2175MM or QOM2175MVH
200A = QOM2200MM or QOM2200MVH

CTA-ID : 15816
Was this helpful?
What can we do to improve the information ?