Technical FAQs

Ask a Question

Are control circuit fuses provided with (Form F4T) devices with control power transformers?

Yes, all control circuit fuses are provided as standard. However, please note that if device is fusible type combination power fuses are not included.


CTA-ID : 15273
Was this helpful?
What can we do to improve the information ?