Technical FAQs

Ask a Question

What size of mounting screw is used with the PK15GTA6 equipment ground bar?

Issue:
Product Features

Product Line:
QO and HOM LC Accessory

Cause:
Clarification of screw size

Resolution:
Two different sets of mounting screws are supplied with the PK15GTA6. One set is 8-32 x .750``. The other set is 10-32 x.375``. All are pan head (phillips drive) THREAD FORMING screws. Do not substitute a SELF TAPPING screws. To purchase the mounting screws, order part numbers 2159414241 (2 required) and 2159417121 (2 required).


CTA-ID : 15272
Was this helpful?
What can we do to improve the information ?