Technical FAQs

Ask a Question

What size of mounting screw is used with the PK18GTAL equipment ground bar?

It is an 8-32 x .938`` pan head (phillips drive) THREAD FORMING screw. Do not substitute a SELF TAPPING screw. To purchase the mounting screw, order part number 2159414302 (2 required).


CTA-ID : 15270
Was this helpful?
What can we do to improve the information ?