Technical FAQs

Ask a Question

What are the sizes of the XVB conduit entry holes ?

The bottom hole in the XVBC21 is 1 inch or 25 mm`s in diameter, with a side threaded hole approximately 3/4 inch in diameter and accessible by knocking out a plastic insert . A XVBC00 1/2`` NPT adapter is available to fit in the bottom and a XVBC14 cable adapter is available for the side.


CTA-ID : 15535
Was this helpful?
What can we do to improve the information ?