Technical FAQs

Ask a Question

What size of mounting screw is used with the PKOGTA6 equipment ground bar?

It is an 12-24 x 1.125`` slotted pan head machine screw with an internal tooth lock washer. To purchase the mounting screw, order part number 2192218360 (2 required).


CTA-ID : 15267
Was this helpful?
What can we do to improve the information ?