Technical FAQs

Ask a Question

What size of mounting screw is used with the PKOGTA2 equipment ground kit?

It is an 12-24 x .640`` hex/slot washer head THREAD FORMING screw. Do not substitute a SELF TAPPING screw. To purchase the mounting screw, order part number 4020506501 (1 required).


CTA-ID : 15266
Was this helpful?
What can we do to improve the information ?