Technical FAQs

Ask a Question

Does the interior catalog number QON442MS300 have copper bus?

Issue:
Previous design product features

Product Line:
QO Load Centers

Resolution:
This load center interior had tin plated copper connector fingers attached to tin plated aluminum bus. BUT this catalog number is obsolete, NLA and would need to be replaced with the current designed load center.
 
Was this helpful?
What can we do to improve the information ?