Technical FAQs

Ask a Question

What is the main lug wire range of an HCW2359-8 main lug panelboard?

Actual lug size is Qty 4, 3/0-750kcmil AL/ CU, UL wire bending space is Qty 4, 3/0-500kcmil. (Per NEC Table 312.6(B), wire bending space required for (4) 500MCM per phase is 16``. The panel has 16.32`` of wirebending space at mains end.)


CTA-ID : 15512
Was this helpful?
What can we do to improve the information ?