Technical FAQs

Ask a Question

What are the dimensions on a Homeline Value Pack HOMVP1 200 amp?

Issue:
Product features

Product Line:
 Homeline load centers

Environment:
Dimensions

Cause:
application and installation

Resolution:

The HOMVP1 includes a HOM3040M200TC load center, which is 14.25`` W x 33.78`` H x 3.75`` D. 

CTA-ID : 15508
Was this helpful?
What can we do to improve the information ?