Technical FAQs

Ask a Question

Is ZCKM1H7 the whole limit switch or the actual body without head?

ZCKM1 is the body without a head, the H7 sets the conduit entry at 1/2 inch NPT


CTA-ID : 15507
Was this helpful?
What can we do to improve the information ?