Technical FAQs

Ask a Question

Can a QON442MS400 load center be either top or bottom fed?

The interior is set up for bottom feed as standard. For a top feed application, first rotate the main breaker 180 degrees, then rotate the entire load center interior 180 degrees.
NOTE: When the interior is rotated, the deadfront trim labels will be upside down. The labels should, if handled carefully, be able to be removed and repositioned for proper orientation.


CTA-ID : 15241
Was this helpful?
What can we do to improve the information ?