Technical FAQs

Ask a Question

On a XCSE7311 what is the adaptor that goes from 13 mm metric conduit to standard 1/2`` conduit? <br />

Use; DE9PA3132A - 13 mm metric conduit for 1/2`` standard conduit. XCSE... can be ordered with 1/2 inch NPT by changing the last digit to 3. ex. XCSE7313 would be 1/2 inch NPT as standard.

CTA-ID : 14967
Was this helpful?
What can we do to improve the information ?