Technical FAQs

Ask a Question

Can the NEMA Class 8502 contactor be converted to a starter by installing an overload relay?

The NEMA size 00, 0, & 1 can be converted by ordering the appropriate replacement overload relay. However, due to base-plate differences between the contactor and starter NEMA size 2 and above will require a separate mount type overload for this conversion.


CTA-ID : 14960
Was this helpful?
What can we do to improve the information ?