Technical FAQs

Ask a Question

When replacing a QE2200VH with a QE2100VH in an EZM Meter Center, what is required to cover the space left by the smaller frame QE2100VH breaker?


Product Line:
Obsolete EZM

Breaker replacement

Nothing additional is required to cover the empty space. When you place the cover back on the device, the empty space created by the smaller frame QE-VH breaker will be covered. Once the cover is replaced, there will be no noticable difference. Please also be aware that the lug orientation of the two breakers are different. The lugs are oriented out the ON end (top) of the QE2200VH, while the lugs are oriented out the OFF end (bottom) of the QE2100VH. Always place the QE2100VH with the ON position up, OFF position down.

CTA-ID : 15498
Was this helpful?
What can we do to improve the information ?