Technical FAQs

Ask a Question

What is required to use Class J fuses in a PS200A plug-in unit?

You will need to adjust the load base assembly from the Class H position to the Class J position as described in the installation instructions provided with the unit.

CTA-ID : 14942
Was this helpful?
What can we do to improve the information ?