Technical FAQs

Ask a Question

9007R18, what is this.<br />

This is a roller only, must be mounted on a 1/4`` keystock or 3/16 rod. Use this in conjunction with R16 or R17 clamp



CTA-ID : 15746
Was this helpful?
What can we do to improve the information ?