Technical FAQs

Ask a Question

Does the HOM1632U200TC load center have copper bus?

Issue:
Does the HOM1632U200TC load center have copper bus?

Product Line:
QO and Homeline Load Centers

Environment:
Determining what material is used for the bus bars

Cause:

Meet specifications

Resolution:

No, this load center uses tin plated aluminum bus.



CTA-ID : 15206
Was this helpful?
What can we do to improve the information ?