Technical FAQs

Ask a Question

Does 2510 manual starters have to be manually reset if power is lost?

No, these devices use maintained controls that are locked in place until manually activated. If true manual device is need and required to drop-out when power is lost; consider the GV2ME IEC starters with the addition of under voltage trip module. Otherwise, see suggested replacements for the obsolete 2510 devices with low voltage protection (LVP).

CTA-ID : 15200
Was this helpful?
What can we do to improve the information ?