Technical FAQs

Ask a Question

Does the QO24L60NRNM load center have copper bus?

Issue:
Product Feature

Product Line:
QO LC

Cause:
Copper buss feature

Resolution:
No, this load center uses tin plated aluminum bus. A copper bus equivalent is not available in the non metallic enclosurre. 


CTA-ID : 14922
Was this helpful?
What can we do to improve the information ?