Technical FAQs

Ask a Question

What is the ambient temperature rating for the 2510M starters?

Per the Nema standards the ambient temperature rating is 0-40 degrees C.


CTA-ID : 15744
Was this helpful?
What can we do to improve the information ?