Technical FAQs

Ask a Question

Is a 200% neutral required in an NQOD panelboard with a TVSS unit mounted internal in the panelboard?

Non-linear or 200% neutrals are no longer provided as standard when a tvss panel is built with the tvss unit mounted internal to the panel. They are available as an option when specified by the customer.

Reviewed 3/10/04


CTA-ID : 15727
Was this helpful?
What can we do to improve the information ?