Technical FAQs

Ask a Question

What is the part number for the copper version of an HCW8SN?

40517-428-51 (copper base w/ aluminum lugs)

HCW8SNCU (copper base w/ copper lugs)



Revised 4/27/04



CTA-ID : 15722
Was this helpful?
What can we do to improve the information ?