Technical FAQs

Ask a Question

What is the copper version of an HCW6SN neutral?

A 40517-427-51 is a standard copper neutral w/AL lugs.
An HCW6SNCU is a copper neutral w/CU lugs.


REJECTED: REFER TO FAQ 2004287



CTA-ID : 15721
Was this helpful?
What can we do to improve the information ?