Technical FAQs

Ask a Question

Can the cover of a LA400S, Series E01, E02 or E03 surface mount circuit breaker enclosure be changed to adapt the enclosure to a flush mount application?

The cover from a LA400F will physically fit onto the LA400S enclosure. A replacement cover ordered as a repair part would not include any labeling nor wiring diagram. Since the UL manifest is located on the wiring diagram, this change is not recommended.

CTA-ID : 15175
Was this helpful?
What can we do to improve the information ?