Technical FAQs

Ask a Question

Are the 9001 SK operators rated for a ``Wash Down Condition``?

The 9001 SK line is rated for NEMA 4 and 4X. NEMA 4/4 X is resistant against low pressure hose down.


CTA-ID : 15702
Was this helpful?
What can we do to improve the information ?