Technical FAQs

Ask a Question

What form is used to order 50 degree C calibrated circuit breaker KAL36225

Use the suffix -35, ie KAL36225-35. These breaker are not UL listed


CTA-ID : 15430
Was this helpful?
What can we do to improve the information ?