Technical FAQs

Ask a Question

What is voltage code V99?

This voltage code is used when the desired coil voltage does not have a published code, and the desired coil voltage should be specified immediately after the catalog number of the starter when an order is placed. This code has restricted use. The voltage in question must be verified by the factory before using.

CTA-ID : 14863
Was this helpful?
What can we do to improve the information ?