Technical FAQs

Ask a Question

What is the correct orientation of the ME25CT2 neutral current transformer?

A. Primary
If load is connected to OFF end of circuit breaker, connect load
neutral to H1 terminal of neutral CT.
If supply power is connected to OFF end of circuit breaker, connect
supply neutral to H1 terminal of neutral CT.
B. Secondary
Connect terminals X1 and X2 of neutral CT to terminals 1 and 2,
respectively, of the circuit breaker terminal block, using no more
than 25 ft. (7.6mm) of No. 14 AWG (2.5mm2) wire.


CTA-ID : 14861
Was this helpful?
What can we do to improve the information ?