Technical FAQs

Ask a Question

9007MS04S0100 - received with the rotary head. It had no lever arm. Is this correct?<br />

This should be complete device without the lever. The lever should be ordered separately.



CTA-ID : 15677
Was this helpful?
What can we do to improve the information ?