Technical FAQs

Ask a Question

What lugs are included in the MMLK250 kit?

The kit includes three double barrel lugs (for both phases and neutral). Each lug will accept (1) #1/0 - 600 kcmil or (2) 1/0 - 250 kcmil conductors.


CTA-ID : 15135
Was this helpful?
What can we do to improve the information ?