Technical FAQs

Ask a Question

What is the control coil voltage operating range of the LC1D contactor?

For 50/60 hertz coils 85% to 110% of rated voltage..
For 50 or 60 hertz coils 80% to 110% on LC1D09** through LC1D32** and 85% to 110% on LC1D4011 through LC1D15000 of rated voltage.


CTA-ID : 15129
Was this helpful?
What can we do to improve the information ?