Technical FAQs

Ask a Question

What is part # for a 20 amp 2 phase Homeline Breaker with a Switch Neutral?

Switch Neutral Breakers are not offerred in the Homeline Style. This is offered in the QO style as a QO320SWN for two hots and one neutral.

CTA-ID : 15123
Was this helpful?
What can we do to improve the information ?