Technical FAQs

Ask a Question

Is the 92346 HP rated?

The 92346 is not HP (horsepower) rated. It is not load make/load break rated and should not be used for a motor load application.


CTA-ID : 15118
Was this helpful?
What can we do to improve the information ?