Technical FAQs

Ask a Question

What Tenant Circuit Breakers can be used with a EZM114200 Series M01 Meter Center?

Issue:
Product Design Features

Product Line:
EZ Metering Equipment

Environment:
Tenant breakers

Cause:
Application/Installation

Resolution:
This EZM114200 Branch device, uses Q2M, Q2M-VH or Q2MH, 100 through 200 ampere, tenant circuit breakers. Example Catalog Number for 200 ampere - Q2M2200, Q2M2200VH or Q2MH2200. For 40 through 125 ampere requirements, the Q2M can be substituted with an EZM125QOA adapter and a QO, QO-VH or QOH, 40 ampere through 125 ampere, tenant circuit breakers. Example Catalog Number for 60 ampere - QO260, QO260VH or QOH260.

NOTE: If Considering the EZM120QOA PLEASE VERIFY THE SHORT CIRRCUIT CURRENT RATING BEFORE USING.
 
Was this helpful?
What can we do to improve the information ?