Technical FAQs

Ask a Question

What are the repair parts for the 92351, series T4 (may be shown as T04)?

The repair parts for the 92351, series T4 (T04) are as follows. No other parts are available.
-Line Base Assembly - 70238-181-50 (requires one per phase. Includes plastic base, switching blade and switch jaws, line and load lugs. NOTE: crossbar insulator should also be replaced)
-Crossbar Insulator - 70238-177-02 (requires one per phase)
-Line Base mounting screws - 21532-171-41 (requires 2 per line base)



CTA-ID : 15917
Was this helpful?
What can we do to improve the information ?