Technical FAQs

Ask a Question

What are the repair parts for the 92251, series T4 (may be shown as T04)?<br />

The repair parts for the 92251, series T4 (T04) are as follows. No other parts are available.
-Line Base Assembly - 70238-181-50 (requires one per phase. Includes plastic base, switching blade and switch jaws, line and load lugs. NOTE: crossbar insulator should also be replaced)
-Crossbar Insulator - 70238-177-02 (requires one per phase)
-Line Base mounting screws - 21532-171-41 (requires 2 per line base)



CTA-ID : 15916
Was this helpful?
What can we do to improve the information ?