Technical FAQs

Ask a Question

What are the style K levers for the L140 Emergency (Maintained stop) cable pull.?

KA - 1.5 inch length.
KO - 2.5 inch length.
KB - 3.0 inch length.
Note: Order Type number only no Class number is needed.

CTA-ID : 15644
Was this helpful?
What can we do to improve the information ?